Back to Main Menu

Introduction to Accounting

Assetic Accounting is designed to act as an asset sub-ledger, enabling double-entry book-keeping at an asset component level. Using Assetic Accounting an organisation can recognise, depreciate, capitalise, revalue, track operating expenses and dispose of asset components via a range of transactions. The module is designed to integrate with ERP and Finance systems.

 

The module supports two methods of asset accounting:

 

The system allows an organisation to run both ledgers simultaneously if required.